TOSHIBA EA60-155 blue screen "ACPI COMPILANT..."

Reply
Member
Posts: 3

TOSHIBA EA60-155 blue screen "ACPI COMPILANT..."

[ Edited ]

hi,there.

here i have TOSHIBA EA60-155 MODEL NO:  PSA67E - 00300C8J

recently happen with the blue screen "ACPI COMPLIANT..." when boot up after "winxp wave icon"

as below display:

i have tried reinstall with winxp cd disc.cannot procees with unsuccess....freeze or blue screen..

i have tried update the bios,follow the "http://laptopforums.toshiba.com/t5/Drivers-and-Utilities/Equium-A60-BIOS-Update-Problem/td-p/99434"

but i got the error ,as below display

any one can help ??

Posts: 47,981
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: TOSHIBA EA60-155 blue screen "ACPI COMPILANT..."

 

Equium A60-155 (PSA67E-00300C8J)

 

Bug Check 0xA5: ACPI_BIOS_ERROR 

 


i have tried update the bios, ... but i got the error ,as below display


To run Osaka20V190.exe Windows must be running. Checkmate.

 

Sorry, I can't help.

-Jerry
Channel 9
Occasional Contributor
Posts: 16

Re: TOSHIBA EA60-155 blue screen "ACPI COMPILANT..."

one thing you try is when u boot up boot in safe mode, then unistall the windows and you said u have the disc so jus reinstall the os or windows thats my best answer sorry  i cant tell you how though

Member
Posts: 3

Re: TOSHIBA EA60-155 blue screen "ACPI COMPILANT..."

thanks for reply ,mate

that's not good method.i did all of them before i postSmiley Sad

i want to know the error on update bios...