Satellite L505D-GS6000 won't boot up, black screen, unresponsive

Reply
Member
Posts: 2

Satellite L505D-GS6000 won't boot up, black screen, unresponsive

I own a Satellite L505-GS6000 that has decided that it no longer feels compelled to respond to my commands. I was using the machine earlier this evening when I decided it was time to feed my family, so I locked my screen to keep the kids off of it, closed the laptop, and left it on the table. When I returned to boot it back up again, I opened the machine and it did nothing. I hit the power button thinking it needed further prompting beyond just opening it to wake up and still nothing happened. I kept trying the power button but nothing happened. 

Since I don't keep my battery in the computer when I'm plugged into the wall, I pulled the chord from the side and waited a few seconds before plugging it back in. After plugging it in, I hit the power button again and it started running the fan so I thought it was going to boot up. Nothing happened beyond a black screen and some fan noise. I attempted all sorts of different things like using battery power instead, using both the chord and the battery, plugging a flash drive into one of the ports, and finally I took the battery out, disconnected the chord, and held the power button for a couple of minutes to discharge any power in it while I Googled the problem from my iPod touch. Still nothing but the fan. 

So here I am, on my husband's laptop researching whether or not I need to weep over lost data. 

One more thing to add, the a/c power light comes on when plugged into the wall, the battery power light comes on when it's in the laptop, and the power button comes on when I try to turn on the machine, but the internal storage light remains dark (along with the memory card reader light that I'm obviously not trying to use at this point anyway.) 

I have a feeling that this is a good indication that either my hard drive needs replaced or that the motherboard needs fixed. At least that's what my brother the IT guy says without knowing anything about Toshiba laptops. Can anyone help a girl out here? Much appreciated. 

Posts: 1,735
Topics: 48
Kudos: 888
Solutions: 135
Registered: ‎10-22-2011

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

It sounds as though the motherboard either needs serviced or replaced.  I have bought several systems with the exact same symptoms, and in every case, it was the motherboard.  Don't worry, I doubt you have lost anything from your hard drive.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 2

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

Update: I took it to Best Buy where I bought it and let the "Geek" behind the counter assess the situation. It was indeed the mother board, but I'm being charged $100.00 that I don't really have to pull my data from the hard drive. Looks like I'll be shopping for a new laptop. Smiley Sad Could be worse though. 

Thanks for your reply!

Posts: 1,735
Topics: 48
Kudos: 888
Solutions: 135
Registered: ‎10-22-2011

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

DON'T SPEND $100 for them to pull your data!!!  You can get a SATA HDD to USB cable on ebay for $5-10, and get the data yourself.  Not worth spending the money for them to do it.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 1

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

If Laptop Will Not Start Up (Power, Battery, AC Adapter LEDs ON, NO Hard Drive Activity LED, NO Display,

NO F2, ESC, etc)

 

01.  Power OFF Laptop

02.  Unplug USB Laptop chiller fan

03.  Battery is installed

04.  Plug-in AC Adapter

05.  Power ON Laptop

06.  Wait 15-60 minutes!!

07.  Power OFF Laptop

08.  Unplug AC Adapter

09.  Power ON Laptop (Laptop should Start Up!)

10.  Plug-in AC Adapter

11.  Plug-in USB Laptop chiller fan (Laptop chiller fan required otherwise CPU will overheat and HALT system)

 

Above steps have worked every time my Toshiba L505D-GS6000 Laptop would not start up.

 

Member
Posts: 1

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

This really Worked!!!!!!!!! minus the fact I dont have a laptop chiller fan,followed steps,I will be honest and thought

the motherboard went,I noticed the fan was the only thing coming on(ablet slow) waited about 20 min it powered

down by it self which I thought was odd but hit the power button and she fired up

Member
Posts: 1

Re: Satellite L505D-GS6000 won't boot up, black screen, unresponsive

Thank you for the fix, but this fix is over two years old, I'll admit I was suprised it actually worked.  My big question is, if this is a known problem with Toshiba laptops, there has to be a way to fix this from happening again.  I had to try this trick twice to get it to work, only reason I can think of as to why it took two tries was maybe the battery wasn't fully charged the first time.

There has to be some sort of way to prevent the Laptop from doing this again in the future.  But seriously, thank you for this fix, while i can handle the occasional PC Lockup, this is my wifes laptop, and I can't always be there when her Toshiba tanks.

 

Dave Smiley Happy