Satellite C675 -S7200 blank screen

Reply
Member
Posts: 4

Satellite C675 -S7200 blank screen

I will retry to explain as best as I can
About 2 days ago my laptop exited out the sight that I was and I try to load up Internet explore but it says it's not valid. Then I go to shut down and it didn't shut down it was still at the main screen so then I had to do a hard reboot. I try and turn it back on but every time I turn it on I go to the blank screen but I can press f2 and go to the boot menu. That's about all I can do please help me fix this problem.
Posts: 47,960
Topics: 85
Kudos: 9,135
Solutions: 3,232
Registered: ‎12-04-2008

Re: Satellite C675 -S7200 blank screen

 

Satellite C675-S7200

 

 

Can you reach the Windows Recovery Environment starting with F8?

 

   What are the system recovery options in Windows 7?

 

If so, try a System Restore first.

-Jerry
Channel 9