Reply
Member
Posts: 1

Page freeze

Having probs with page freeze when using my USB dongle for 3g. Contacted 3g and they say it is prob with my laptop. Using windows7 upgrade, had no probs when on vista, any help would be grateful

Member
Posts: 1

Re: Page freeze

Hi,

 

I have the same problem: win 7 on a Portégé M700 freezes while using the 3G connection, irrespective if the SIM card is installed in the internal slot or I use an external USB dongle.

 

It was working fine, then suddenly yesterday I noticed this behaviour. I recently installed the HDD protection driver (not installed before) e and few other drivers, like the Samsung universal printer driver, but I do not have evidences of a relationship with one of them, up to now.

 

I have XP installed in the same M700, which is working fine with the same hardware, so that I suspect a software issue.