Re: P855 S5200 Keyboard

Reply
Member
Posts: 4

P855 S5200 Keyboard

My keyboard does NOT work when I get to my login screen -- but if I restart the computer then it works... What the.....???????

Posts: 4,901
Topics: 57
Kudos: 1,686
Solutions: 386
Registered: ‎05-03-2009

Re: P855 S5200 Keyboard

Try the following, Karl.

 

1.  Open Device Manager, double click on Keyboards, right click the Internal Keyboard and click Uninstall.  Restart computer and the Keyboard driver will be automatically reinstalled.

 

2.  If that doesn't cure your problem, do a System Reset.  Turn off computer. Remove all attachments and battery. Press and hold the Power button for 15 seconds.  Attach Power and insert battery.  Start computer and tap F2 at the Toshiba splash screen to get in BIOS.  Press F9 to setup system defaults. Answer Yes. Press F10 to Save Configuration Changes and Exit.  Answer Yes to complete the process.  The computer will restart.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 1

Re: P855 S5200 Keyboard

try taking the battery out, i had that problem once, never happened again
Posted from Facebook
Highlighted
Member
Posts: 4

Re: P855 S5200 Keyboard

I will do ANYTHING you say, Tiffany! Smiley Very Happy

 

I think the battery thing solved the problem - AND, I put a nice Intel SATAIII SSD in so it's really fast now!