Notebook isn´t working anymore

Reply
Highlighted
Member
Posts: 1

Notebook isn´t working anymore

Hi,

my problem: I have a notebook which isn´t working anymore. The LED, which shows me that the battery is loading and the one for power plugin are shining a little bit.
When I want to start it the LED of caps lock is shining for a short time. Also the LED of the power button is shining. Holding this a little bit to shut the system down it will go out.
That means it must be working or?

But there is nothing on the display, the drive isn´t working and you can´t here a fan or hard drive. So it is completly quiet only the 2-3 LEDs are working.


Any idea what this could be?

Thanks

Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: Notebook isn´t working anymore

Turn off your laptop, unplug all wires, remove the battery, and hold the power button for thirty seconds. Afterwards, reattach the battery and connections.

 

If it still doesn't work, it sounds like it would require servicing. You can contact customer support at (800) 457-7777.

- Peter