New Toshiba L850 Blue Screen Of DEATH!!

Reply
Highlighted
Member
Posts: 2

New Toshiba L850 Blue Screen Of DEATH!!

Well I just purchased this baby on the 28th of august and now its the 14 of september and ive gotten the blue screen of death multiple times. I have tried restoring it with the backup i made when i first booted it and tried system repair. I have never droped it or anything. Im wondering if I have a Bugged one with a falty hard drive or something? So any sugestions how i can fix or should I just send it back to  toshiba or the store I bought it from (Staples) 

 Thanks for your guys time.

Posts: 4,808
Topics: 56
Kudos: 1,534
Solutions: 370
Registered: ‎05-03-2009

Re: New Toshiba L850 Blue Screen Of DEATH!!

 

"I have tried restoring it with the backup I made when I first booted it"

 

Since that didn't work means there is something inherent in the machine causing the problem.  I would return it where I bought it.  If it's too late for that, call Tech Support at 1-800-457-7777.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit