NB205 Netbook- replace hard drive

Reply
Member
Posts: 2

NB205 Netbook- replace hard drive

Be gentle, since I'm not very technical.....

 

I was preparing my rarely used Netbook (XP version) to give to my elderly father & installed AVG with current virus definitions with no problem.  When I went to upgrade to the current version of Firefox, it hung.  When I tried to reboot, it wouldn't & started clicking.  From what I've been told, the hard drive probably crashed & needs to be replaced.  Any other ideas?

 

If that's all it is, will any SATA 2.5 work & can I go to 7200 vs 5400?  Since I never created a restore disc (no CD drive), do I have to buy from Toshiba?

 

And are there directions for replacing the hard drive, since I hope to do it myself?

 

Thanks!

 

Karen in Texas

Posts: 48,235
Kudos: 9,199
Solutions: 3,265
Registered: ‎12-04-2008

Re: NB205 Netbook- replace hard drive

Which NB205, Karen?

 

I've attached some pictures to help you replace the disk. You will re-use the existing caddy ("plate" in the picture).

 

You will need to order the recovery discs from Toshiba.

 

   Order Toshiba Recovery Media

-Jerry
Channel 9
Member
Posts: 1

Re: NB205 Netbook- replace hard drive

What size torx wrench/drive do I need to remove the cover on the NB205 to access the HDD and where can I purchase the correct tool?

Member
Posts: 1

Re: NB205 Netbook- replace hard drive & install software

I saw this  old thread, and thought I'd post here.

 

It seems the HDD on my Toshiba NB205 has died.  I never backed it up, but no big loss of data.  However, I have no recovery disks that I know of, nor do I have an external dvd drive.

 

So, even if I buy and install a new HDD, how would I get Windows installed, and all the Toshiba software installed?

 

Thanks

Posts: 4,934
Topics: 57
Kudos: 1,735
Solutions: 389
Registered: ‎05-03-2009

Re: NB205 Netbook- replace hard drive & install software

Next time you post on the Forums, please start your own thread rather than piggy back on  another--in this case, one over a year old!  Recovery Media is also available in USB form.  I'm not sure about your specific machine. Go HERE and scroll down to order.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit