My Toshiba laptop is running slow while internet browsing

Reply
Member
Posts: 1

My Toshiba laptop is running slow while internet browsing

I think my laptop just needs to be "cleaned up"

It seems like it's been running more slowly over time.  I used customer service once to clean it up once, and it ran much better.  Now my warranty has expired and I can't recall the steps to clean it up.

I mostly use it for browsing using Internet Explorer.  I also download pictures from my digital camera.

Any help would be appreciated.

Thanks

Posts: 4,813
Topics: 56
Kudos: 1,537
Solutions: 370
Registered: ‎05-03-2009

Re: My Toshiba laptop is running slow while internet browsing

CCleaner is a free download that I have used for many years to keep the crap from building up in my computer. Be sure and click on the Free Download box to the left of the window I linked you to. If you ever have occasion to post back here, please include your model info as in in my examples below.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 45,957
Topics: 81
Kudos: 8,253
Solutions: 3,088
Registered: ‎12-04-2008

Re: My Toshiba laptop is running slow while internet browsing

Always tell us which computer you have when you post here. There is a label on the bottom.

 

If your problem involves the browser, tell us which one.

 

This is for Internet Explorer.

 

   Is Internet Explorer slow? 5 things to try

 

"Cleaning things up" on the hard drive or in the registry is unlikely to help your browsing speed.

-Jerry
Channel 9