How to remove DVD drive on Toshiba P770D laptop ?

Reply
Member
Posts: 1

How to remove DVD drive on Toshiba P770D laptop ?

How you remove DVD drive on this Toshiba laptop? There's one screw but after it's removed the bay will still not pull out.

 

Does anybody know if the entire back side has to be unscrewed?

 

Or does the keyboard specifically have to be removed in order to remove the DVD drive because there's a screw also inside?

Posts: 1,735
Topics: 48
Kudos: 889
Solutions: 135
Registered: ‎10-22-2011

Re: How to remove DVD drive on Toshiba P770D laptop ?

Turn on the computer, eject the DVD drive, then shut down.  Flip the laptop over, and remove the battery.  Remove the screw to the left of the Toshiba sticker(screw is flush compared to the other screws).  Pull outward on the DVD drive, and it should pull right out with little effort.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD