How to Use the Print Screen Button (PRTSC)

Reply
Member
Posts: 5

How to Use the Print Screen Button (PRTSC)

I had an Older  Model that had a Seperate Button Now I Have the Satelite  L775d- S7132

The Button is on The Same Button To Scroll to Bottom of Page (END)

I Called  the Toshiba Support  But He Did  NOT HELP ? Id sendaPicture If I knew How i could Not Find  it in the GUIDE

Posts: 4,934
Topics: 57
Kudos: 1,734
Solutions: 389
Registered: ‎05-03-2009

Re: How to Use the Print Screen Button (PRTSC)

[ Edited ]

Hold the FN key down and press "PRTSC" and the screen is copied to the clipboard. See page 104 of your User's Guide.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 48,228
Kudos: 9,198
Solutions: 3,265
Registered: ‎12-04-2008

Re: How to Use the Print Screen Button (PRTSC)

[ Edited ]

Adding to CB's accurate post (from p. 104)..

 

   

 

 


I Called  the Toshiba Support  But He Did  NOT HELP ?


I wonder why. This is an easy on.

-Jerry
Channel 9