Reply
Member
Posts: 2

Creating Recovery Discs for C655-S5212

Apologize if this has already been asked/answered.  I did search first.

 

I'm trying to run the utility to create recovery discs for my daughters new Satellite C655.  Only one of the 4 DVDs created without some type of error.  The error I received on the last DVD said "failed to read the following file D:\sources\boot.wi  error code 020150-20-0000000

 

The other errors were different but I didn't write them down.  I'm very frustrated as I've wasted about 4 DVDs at this point trying to run the process error free.

 

 

Member
Posts: 2

Re: Creating Recovery Discs for C655-S5212

Should have mentioned, the process did burn files to each of the DVDs.  My concern is whether all of the data is there and will work when/if we need it.