Cannot access Toshiba HWSetup

Reply
Occasional Contributor
Posts: 14

Cannot access Toshiba HWSetup

When I tried to access Toshiba HWSetup in XP's Control Panel, I got the following error message:

Common Module terminated!

I have not the foggest idea what does that mean. Is there any way to get around it? Thanks for your time to read this post.

Posts: 46,788
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Cannot access Toshiba HWSetup

Which computer? There is a label on the bottom.

-Jerry
Channel 9
Occasional Contributor
Posts: 14

Re: Cannot access Toshiba HWSetup

Sorry I forgot to mention. It's To**bleep**a Satellite M45-S265. The reason I tried to access To**bleep**a HWSetup is the power button doesn't work properly. It's function has been replaced by the internet button. In other words, I have to use the internet button to turn the laptop on/off. The power button's only function is to show whether the laptop is on (lit) or off (not lit). Actually I'm not sure whether I can solve this problem through Toshiba HWSetup.

Posts: 46,788
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Cannot access Toshiba HWSetup

 

Satellite M45-S265

 

 

Try reinstalling these two utilities in this order.

 

   Toshiba Common Modules for Windows XP

 

   Toshiba Utilities for Windows XP

 

 

You can choose what the power button does in Power Saver.

 

  

-Jerry
Channel 9
Occasional Contributor
Posts: 14

Re: Cannot access Toshiba HWSetup

Thanks for the instructions.

Do I have to download these programs? I checked the Recovery and Applications/Drivers DVD coming with the laptop but could not find them. The only close hits are two folders called Toshiba Common Modules 2 and Toshiba Utilities 2, where sit two executable files, B229900.exe and Setup.exe, respectively.

Posts: 46,788
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Cannot access Toshiba HWSetup


Do I have to download these programs?


Yes, download and then execute each of those programs in turn.

 

The first one reinstalls the Common Modules and the second one reinstalls the HWSetup utility (which enables you to change settings in the BIOS).

-Jerry
Channel 9