Can't eject the CD/DVD drive

Reply
Member
Posts: 7
Accepted Solution

Can't eject the CD/DVD drive

Could som1 assist in helpin eject CD driver without any inserted CD/DVD?
Occasional Contributor
Posts: 30

Re: Can't eject the CD/DVD drive

try to eject the disc in BIOS (press f2 on the splash screen)...

 

if this one failed, as well as the emergency eject button, your computer needs to be repaired or the drive needs to be replaced...

View solution in original post


All Replies
Frequent Advisor
Posts: 824

Re: Can't eject the CD/DVD drive

Does it not eject with the button on the drive? If that doesnt work, try to poke the emergency eject button, a small hole on the DVD drive.
Member
Posts: 7

Re: Can't eject the CD/DVD drive

Have been trying but couldn't work
Member
Posts: 3

Re: Can't eject the CD/DVD drive

Is it because you have a cd stuck inside the drive? You'll have to play around with the drive if it's detacable by that I mean maybe shaking to loosen the cd that might be stuck or caught inside the drive.
Member
Posts: 7

Re: Can't eject the CD/DVD drive

Thanks for your endevour; have done everything and still helpless.
Frequent Advisor
Posts: 824

Re: Can't eject the CD/DVD drive

If it is still under warranty call Toshiba for your repair options. I think the drive needs to be replaced already.

Administrator Administrator
Administrator
Posts: 2,325

Re: Can't eject the CD/DVD drive

No need to call for repair options.  They are available at http://pcrepair.toshiba.com.

 

Jim

 

Member
Posts: 24

Re: Can't eject the CD/DVD drive

I just want to be sure and I know this was mentioned before.  Did you try the emergency eject hole?  It is a smalle hole that only a paper clip end can fit through.  Use a paper clip to press the hidden button.  This button is different then the big button you can press with your finger that is on the drive to eject the disc.
Occasional Contributor
Posts: 30

Re: Can't eject the CD/DVD drive

try to eject the disc in BIOS (press f2 on the splash screen)...

 

if this one failed, as well as the emergency eject button, your computer needs to be repaired or the drive needs to be replaced...

Member
Posts: 7

Re: Can't eject the CD/DVD drive

Confirmed that the drive needs replacing.

 

Issue resolved and thanks to all who contributed.


Memeo68