CD stuck inside the laptop

Reply
Member
Posts: 1

CD stuck inside the laptop

I have inserted a cd into my laptop but didn't place in in the tray correctly and the cd somehow fell inside and got stuck literally inside the laptop. I can open the drive and play other cds and my laptop works fine but that cd is still inside.. It doesn't rattle and I can't shake it out. What can I do??

Frequent Advisor
Posts: 2,022

Re: CD stuck inside the laptop

let us know which model your laptop is and we can probably give you instructions on removing the dvd drive to get the cd

-civicman4-
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Post all info about your laptop and version of windows. We are working on it but still do not have the powers to read your mind.
Occasional Contributor
Posts: 16

Re: CD stuck inside the laptop

if you have a slot feed cdrom drive you shouldnt try to get it out yourself as you might further damage your on accident. if you have a tray model that pops out then if you follow the center of the cdrom drive in toward the base (bottom plastic) of the computer you will likely see a screw. you will only need to remove that one screw on almost all cases and then you can take your fingernail and literally slide the cdrom drive out or eject your cdrom drive and gently slide it out of the base housing that the cdrom sits in. make sure your computer is off and unplugged. if you feel uncomfortable and your notebook is under warranty im sure you could send it in someone else might be able to help you more if thats the route you take. 

Member
Posts: 1

Re: CD stuck inside the laptop

[ Edited ]

Part NoSmiley TongueSBZ1U-04P01Q

Serial No:XXXXXXXXX

 

Toshiba:G66C0002GC10

 

Product key:XXXXX-XXXXX-XXXXX-XXXXX-XXXXX

 

SatelliteSmiley Tongue775D

 

 

please help me

 

 

 

[Moderator edit to remove serial and key.]

Member
Posts: 3

Re: CD stuck inside the laptop

My Toshiba is a satellite p775-s7160. It has a tray for discs, but I don't see the single screw that you are talking about.

 

I did the same thing as the OP, put in a disk without securing it on the rotator, and now it's inside the laptop. The tray ejects fine, but no disc. I can't even see the disc when I shine a flashlight in it, but it's difficult to see anything because I can't completely remove the tray. It plays other discs just fine, but I still want to remove the stuck one.

Member
Posts: 1

Re: CD stuck inside the laptop

The exact same thing happened to me. Laptop A505. Anyone know how to get the CD out of there?

Member
Posts: 1

Re: CD stuck inside the laptop

This has happened me with a Toshiba laptop bought 3 weeks ago - the cd has stayed within the laptop even though the tray ejects.  I have never heard of such an issue happening with other brands. 

Member
Posts: 1

Re: CD stuck inside the laptop

my laptop is an acer and i can't find anything on this situation by them but im having the same problem and i can't get it out...i need to get it out because it's a rental...i didnt put the disc in properly && when i closed it it just fell inside my computer and the tray comes out perfectly and my computer seems to be running just finee...PLEASE HELPP!!!!

Member
Posts: 5

Re: CD stuck inside the laptop

I have the same problem  I have a Toshiba Satellite S75-A7334

How do I get the drive out so I can get the disk out?

How weird.....

Regular Advisor
Posts: 225

Re: CD stuck inside the laptop

On front of the disc tray there is a tiny hole. You can use a paper clip or pin to eject the tray. Its going to feel like your pushing something inside. And that will open the tray

*********Click on Kudos if it helped you. Thanks! ***********
Member
Posts: 5

Re: CD stuck inside the laptop

It's not like that.  I failed to put the disk completely on the wheel with the teeth so it wasn't laying down flat in the drive.  Its stuck above the drive in a space under the keyboard.  I know, dumb thing to do but I did it.

Member
Posts: 5

Re: CD stuck inside the laptop

YAY!  I got it out.  I wrapped a single layer of duct tape to a thin kitchen knife and was able to grip the cd enough to pull it out so I could get my fingers on it.  Optical drive seems to be working fine and my laptop isn't smoking or anything like that.

Regular Advisor
Posts: 1,337

Re: CD stuck inside the laptop

congrats!

L305-S5955, T9300 Intel Core 2 Duo, 4GB RAM, 60GB SSD, Win 7 Ultimate 64-bit
Member
Posts: 1

Re: CD stuck inside the laptop

Just happened to e ..Satellite laptop -cd stuck inside , Tray opens.  shut of computer.. The tray is encased in a metal housing. THE CD IS ABOVE THE HOUSING (under the keyboard) Stick a regular preferably round tip kitchen knife in the opoen cd slot ABOVE the housing to pry the housing down and allow space for the cd to dropo out as you tilt the computer and open cd tray down. Took 5 seconds AFTER i determined that cd wasnt In  the cd housing  but above it.Apparently  if the cd isnt secured in the tray correctly it can jump up and dissapear in the thin slot above the metal housing.   Good luck

Regular Advisor
Posts: 269

Re: CD stuck inside the laptop

[ Edited ]

Same thing just happened on my A505-S69803.    Thanks for the tips about using a kitchen knife.  I will have to try that after I finish burning my CD.   I wondered where the first CD went.    It won't fall out by itself.     lol

 

 

eta:    The disk got up on the top of the frame of the DVD drive, or else got stuck in the actual innards of the laptop frame.  Thje same thing that the post direcect above this describes. 

 

Anyhow,  I took a thin metal nail file, pried the metal frame piece down just a bit, pried at the side of the disk, got the disk gradually worked out so there was enough sticking out to grab onto.     Then I had to keep using the nail file to push down on the frame, the side of it toward the back edge of the laptop, to make enough gap that the disk could be pulled out.   The disk will be all scratched up, but it will come out of that tiny space above the DVD drive itself.   You can see the edges of it shining.   Use a flashlight to locate the disk.

 

The previous posts were correct, that the DVD drive can continue to be used to burn disks while that other disk is stuck in the framework above it.

 

If I had not found this thread via Google, I would have had no idea where the vanishing disk went or how to get it out.   It's unbelievable, haha.

 

irisvista.com site shows how to take laptops apart.   The A505 series, iirc, must be completely disassembled just to remove the DVD drive.    This thread was very helpful.   I don't want to take the laptop apart.

Member
Posts: 2

Re: CD stuck inside the laptop

i have a C55-A5220  running windows 8 what else do you need


sabinkat wrote:

I have inserted a cd into my laptop but didn't place in in the tray correctly and the cd somehow fell inside and got stuck literally inside the laptop. I can open the drive and play other cds and my laptop works fine but that cd is still inside.. It doesn't rattle and I can't shake it out. What can I do??


 

Member
Posts: 2

Re: CD stuck inside the laptop

should I open the bottom of my laptop

Member
Posts: 1

Re: CD stuck inside the laptop

I put my cd into the tray of my laptop and clicked it in. It was then not reading anything on my laptop so I decided to eject the cd and re put it in. When I opened the tray, the cd was gone. I found it under my keyboard of the computer. After trying tons of ways to get it out (a qtip, a knife, my fingers, a credit card), I then wrapped blue scotch tape around a bread knife (make sure to wrap secreuly to avoid losing tape in the computer). I then put the knife into where the cd was stuck and added pressure to attach the tape to the cd, and it easily slid out.

 

Hope this helps!

LN
Member
Posts: 1

Re: CD stuck inside the laptop

Excellent.  Used a very thin antique rounded point knife and worked it just as you suggested.  No tape, just determination.  Took about 3 minutes.  Don't have to call my sons.  yipee, did it myself, thank s to you.

ROW
Member
Posts: 1

Re: CD stuck inside the laptop

THIS IS THE ANSWER. Tried the duct tape solution mentioned in another suggestion above but could not get it flush and sticky side out. Once I bagged that it took me 2-3 minutes. Aside from your epiphany about it being above the housing and not behind the drive tray, the other thing is to tip it quite a bit. You mention tipping it, but for me the key was to tip it a lot. I put it on the edge of a counter, tipped it, then inserted a thin knife and fished around until it slid out about an inch. Then I grabbed it. Before your comment, I was resigned to taking it to a shop... THANKS!