Can't find hard drive capacity in Windows 8

Reply
Member
Posts: 2

Can't find hard drive capacity in Windows 8

Again, Windows 8 confounds me because of the lack of traditional "Start" button. Is there a "My Computer" window where I can see how much storage iss being used or remains on my hard drive? Sign me, "Windows H8ter!

Posts: 47,991
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: Can't find hard drive capacity in Windows 8

File Explorer (the new name for Windows Explorer) has all sorts of new features.

 

But as usual, you can right-click on the drive itself and click Properties. The General tab looks the same to me.

 

               

 

   Windows 8: New File Explorer features

 

   Windows 8: More new File Explorer features

 

   Windows 8: Even more new File Explorer features

-Jerry
Channel 9
Posts: 1,735
Topics: 48
Kudos: 889
Solutions: 135
Registered: ‎10-22-2011

Re: Can't find hard drive capacity in Windows 8

If you right click on the desktop tool bar, you can add a "desktop bar".  This will add computer, control panel, etc... which makes it easy to find some of these things.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD