TOSHIBA Service Station

0 Kudos
Started ‎11-12-2012 by
Modified ‎10-04-2013 by
(66,014 Views)

SERVICE STATION

 

This application allows your computer to automatically search for TOSHIBA software updates or other alerts from TOSHIBA that are specific to your computer system and its programs. When enabled, this application periodically transmits to our servers a limited amount of system information required to perform these updates or alerts. This feature is enabled by default.

 

Installing Service Station

 

If this utility or feature is not installed on your computer, you can verify if it is available for your specific model under "Downloads" on the Toshiba support web site (support.toshiba.com). Not all utilities are available for every model and operating system. When installing any utilities, install the TOSHIBA Value Added Package first.

 

How To: Identifying and locating the correct driver for your device

 

Fixing a "Toshiba Service Station has stopped working" error

 

If you receive this error, please locate the utility on the Toshiba support web site, download it, and reinstall it.

 

How To: Identifying and locating the correct driver for your device

 

Opening Service Station

 

  1. Click the Start menu. On Windows 8, go to the Start screen.
  2. Enter "Service Station" into the search field. On Windows 8, type "Service Station" while viewing the Start screen.
  3. Click "Service Station" in the search results.
  4. Service Station will open.

 

Enabling or disabling Service Station

 

  1. Click the "View Program Access Information" link located under "Last Update" in the lower Left corner.
  2. Toshiba Service Station Access Information window will open.
  3. To disable this application (not recommended) click the disable button. To continue using this application click the enable button.
Contributors