TOSHIBA Disc Creator

0
Started ‎11-14-2012 by
Modified ‎04-25-2013 by

TOSHIBA Disc Creator

DISC CREATOR

 

With TOSHIBA Disc Creator, you can create original audio CDs, data CDs and DVDs, and backup discs of CDs and DVDs. When creating audio CDs, you can collect only your favorite music from multiple music CDs, and a "MyBest" or "Favorites" CD can be created. Moreover, an Audio CD can be created from audio files collected on the hard disk of your personal computer, such as MP3 and WMA files.

 

When creating data CDs or DVDs, you can save your important multimedia and/or document files from your hard disk drive to CDs or DVDs. When using "Disc Backup", you can create backup discs of your CDs and DVDs, or duplicate DVD-Videos that you have created by yourself.

 

More advanced functions, such as image file creating from CDs/DVDs, creation of CDs/DVDs from an image file, and creation of bootable CDs and DVDs, is also supported.

 

If this utility or feature is not installed on your computer, you can verify if it is available for your specific model under "Downloads" on the TOSHIBA support web site (support.toshiba.com). Not all utilities are available for every model and operating system. When installing any utilities, install the TOSHIBA Value Added Package first.

 

To open TOSHIBA Disc Creator:

 

  1. Click the Start menu.
  2. Enter "Creator" into the search field.
  3. Click "TOSHIBA Disc Creator" in the search results.
  4. The TOSHIBA Disc Creator will open allowing you to create media as described above. disc_1.jpg
  5. Select "Advance Menu" for additional options. disc_2.jpg
Contributors