12-20-2012 05:01 PM
12-20-2012 05:03 PM
12-20-2012 09:52 PM
just got it updated on mine...bout time ![]()
12-21-2012 05:40 AM
Still need time to see if it's any more stable. But it did make it through the night with WiFi sleeping with the tablet. Odds of that on the ICS code were slim.
12-22-2012 09:56 AM
Did GUI in JB change to a phone style or did it stay the same as in ICS - navigation buttons in the left lower corner, notifications in the right lower corner?
12-22-2012 11:24 AM
It's the "table style" as expected. Haven't latched it up yet! That's probably a record amount of uptime for the amount of use I've given it. Didn't change any apps. So the Toshiba excuse of blaming the apps seems weaker now.
12-22-2012 11:41 AM - edited 12-22-2012 11:53 AM
The changes that I noticed, is that
The lock screen includes the Google Search and includes additional animations when making a selection.
The Fonts are different.
The notification bar shows more info , like previews of emails etc. GUI is slighty different.
The keyboard typing seems to be alot faster, and no longer sluggish.
The Google Voice search is redone, its faster more accurrate and more intelligent.
Theres more Wallpapers availible.
The brightness/contrast is readjusted, making icons looks more vibrant and colorful. (This might be just my eye sight this morning) But the display looks different.
There are now new animations when switching between apps.
The GUI for Shutdown/Restart looks different.....looks more like my cellphones menu.
The HDMI output now as 3D output options
The Security now has facial recognition for Lock Screen.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.