usb controller driver

Reply
Member
Posts: 7

usb controller driver

I have a Satellite S855D-S5256. I've tried repeatedly to install the USB Controller for the usb3.0 from this website. 

I have downloaded the package from the drivers for my system titled tca0081300a.exe when it goes through its install process the driver status in the bottom right of my screen says driver not found AMD USB 3.0 Controller. it says the program used to install it is in the folder but not the driver itself. It seems ASUS isnt the only company who cannot package drivers properly. i need the AMD USB 3.0 Controller Driver. 

 

Super Advisor
Posts: 4,069

Re: usb controller driver

[ Edited ]

Now you have 3 threads open on the same issue. Now his particular thread, and this one, and this one.

 

Mike

Member
Posts: 2

Re: usb controller driver

I hear ya twice.   I have the same issue, someone please give us an inclination where to find these drivers.


Thanks,

 

Member
Posts: 1

Re: usb controller driver

[ Edited ]

I have the same problem, and I haven't seen any answers to this, even though it's years old

I needed an answer yesterday, not two years from now - help!!

Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: usb controller driver

rose16, what laptop do you have?

- Peter