toshiba satellite L655D-S5050 webcam driver

Reply
Member
Posts: 5

toshiba satellite L655D-S5050 webcam driver

i've discovered i'm not the only one with this problem but i do need a personal solution. i think the origin of this situation is from almost a year ago when i had a serious virus in my computer. i took it to a repair shop and they rebooted the system with microsoft security essentials and windows 7 and everything turned out fine except i no longer had that sidebar where i could access the webcam. now, i've looked through the devices and i can see under imaging devices that the chicony usb 2.0 is installed and enabled and working properly, and i can use the camera through skype, but i have no other way to access it in order to take pictures or whatever else. just wondering if someone might be able to help out with that...

-bryan

Posts: 4,859
Topics: 57
Kudos: 1,631
Solutions: 377
Registered: ‎05-03-2009

Re: toshiba satellite L655D-S5050 webcam driver

Start/All Programs/Toshiba/Utilities/Web Camera Application  and then the sidebar camera controls should be available to you if you hover your mouse near the left side of the screen.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: toshiba satellite L655D-S5050 webcam driver

i don't even have a "Toshiba" section on my all programs list...

Posts: 4,859
Topics: 57
Kudos: 1,631
Solutions: 377
Registered: ‎05-03-2009

Re: toshiba satellite L655D-S5050 webcam driver

You're the first Toshiba owner I ever heard of that didn't!  Lacking that, I can't think of another way to activate the WebCam.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: toshiba satellite L655D-S5050 webcam driver

there must be some way to access it if i can see the device in the device management section, right? maybe if i uninstall it and then reinstall it?

Posts: 4,859
Topics: 57
Kudos: 1,631
Solutions: 377
Registered: ‎05-03-2009

Re: toshiba satellite L655D-S5050 webcam driver

I would certainly try the uninstall/install but I believe all you might have is exactly what you have now.  It certainly can't hurt.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: toshiba satellite L655D-S5050 webcam driver

once i uninstall it and it disappears from the device management list, how do i re-install it?

Posts: 4,859
Topics: 57
Kudos: 1,631
Solutions: 377
Registered: ‎05-03-2009

Re: toshiba satellite L655D-S5050 webcam driver

[ Edited ]

Go here: http://www.csd.toshiba.com/cgi-bin/tais/support/jsp/modelContent.jsp?ct=DL&os=&category=&moid=268156...  Your Webcam Driver is on page 3.

 

I won't be back online until about mid-morning tomorrow.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 5

Re: toshiba satellite L655D-S5050 webcam driver

after uninstalling it and clicking on that link for the driver i can now use my camera! thank you.

Posts: 4,859
Topics: 57
Kudos: 1,631
Solutions: 377
Registered: ‎05-03-2009

Re: toshiba satellite L655D-S5050 webcam driver

That's great news, Bryan!

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit