should I install? BIOS version 1.90 for Satellite A305 ?

Reply
Member
Posts: 1

should I install? BIOS version 1.90 for Satellite A305 ?

Hi

 

I would like to know if someone has already installed the bios, and if it brings some improvements to the system.

I have a Satellite A305-S6916 bought at bestbuy
Sometimes I think the system more time to start
tks.
Posts: 47,950
Topics: 85
Kudos: 9,133
Solutions: 3,230
Registered: ‎12-04-2008

Re: should I install? BIOS version 1.90 for Satellite A305 ?

 

Satellite A305-S6916 

 


I would like to know if someone has already installed the bios, and if it brings some improvements to the system.

I wouldn't update that unless there's something listed that's fixed.

 

   ACPI Flash BIOS version 1.90 for Satellite A305 (PSAGCU/PSAG8U) 

 


..more time to start

Maybe something here helps.

 

   How to troubleshoot performance issues during startup in Windows Vista

-Jerry
Channel 9
Member
Posts: 9

Re: should I install? BIOS version 1.90 for Satellite A305 ?

HAVE SAME LPT I PUT WINDOWS 7RC ON PETITIONED HDD RUNS GREAT HAVE ALREADY ORDERED WIN 7, AS FOR BIOS 1.90 I ASKED TOSHIBA AND THEY WERE NO HELP. THERE ARE SOME CODE REVISIONS IN 1.80 SO I MITE TRY IT BUT I THINK MOST OF THE PROBLEMS WITH A305-S6916 IS VISTA. I RAN BOOT TIME TESTS ON BOTH OS AND VISTA TOOK OVER 3.5 MIN TO GET TO DESKTOP AND WAS STILL LOADING, WERE AS 7RC BOOTS IN 90 SEC. AND YOUR GOOD TO GO.

Member
Posts: 9

Re: should I install? BIOS version 1.90 for Satellite A305 ?

 HAVE PROBLEMS WITH USB PORTS STOPING HAVE FOND NO OTHERS WITH THE PROBLEM BUT FUTHER RESEARCH I FOUND ICH9M CODE UPDATE IN 1.80 SO ITHINK IT IS GOOD IDEA TO DO IF YOU ARE COMFOTABLE WITH THE PROCESS. SUGUEST DOING BOOT INSTALL FROM DISK. I DON;T TRUST VISTA TO DO ANY THING RIGHT.

Regular Advisor
Posts: 3,300

Re: should I install? BIOS version 1.90 for Satellite A305 ?

When your Win7 arrives, just remember you have to deinstall Win7RC first!