Reply
Super Advisor
cbwilsha
Posts: 2,570

Re: need network drivers for Qosmio F60-14F

As Jerry Lippey said in the post just before yours, this is the site for US machines. Yours appears to be a Middle East machine and your drivers are located HERE.

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit
Member
basushaunak
Posts: 1
0

Re: need driver Satellite C640

Where can I find driver for Bluetooth for Win 8 x64 Pro? Tried all the Win7 x64 drivers, they just don't work ('unable to start device' in device manager)...

Super Advisor
cbwilsha
Posts: 2,570
0

Re: need driver Satellite C640

There are no Model C640's sold in the U.S. and as mentioned above several times, this is the site for U.S. machines. If your model IS a U.S. machine, click on Downloads above and follow directions to find your drivers and other support.  If it is not a U.S. machine, contact Toshiba in your part of the world.

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit