cant find sound driver for Portege r205-s209

Reply
Member
Posts: 1

cant find sound driver for Portege r205-s209

I recently got a second hand toshiba protege without the cds and Im unable to get any sound from the pc, Ive been unsuccefully trying to find the drivers on the internet, the toshiba website has no link where I can download the driver.

Are the drivers posted on Intel compatible with toshibas laptops???

add info

toshiba Portege r205-s209

intel pentium m 1.20mhz

 

Can someone tell where I can download the driver for free

info provided by everst home edition

 

Motherboard: CPU Type Mobile Intel Pentium M ULV 753, 1200 MHz (12 x 100) Motherboard Name TOSHIBA PORTEGE R205 Motherboard Chipset Intel Alviso-G i915GMS System Memory 1270 MB (DDR2-533 DDR2 SDRAM) BIOS Type Toshiba (02/14/08) Communication Port Toshiba BT Port (COM15) 

Display: Video Adapter Mobile Intel(R) 915GM/GMS,910GML Express Chipset Family (128 MB) Video Adapter Mobile Intel(R) 915GM/GMS,910GML Express Chipset Family (128 MB) 3D Accelerator Intel GMA 900 Monitor Toshiba Internal 1024x768 Panel (0003) Monitor Toshiba Internal 1024x768 Panel (0003)

Multimedia: Audio Adapter Intel 82801FBM ICH6-M - AC'97 Audio Controller [B-1] Storage: IDE Controller Intel(R) 82801FB/FBM Ultra ATA Storage Controllers - 266F Disk Drive TOSHIBA MK6006GAH (60 GB, 4200 RPM, Ultra-ATA/100) Disk Drive Secure Digital Storage Device SMART Hard Disks Status OK

 

Posts: 45,932
Topics: 81
Kudos: 8,225
Solutions: 3,088
Registered: ‎12-04-2008

Re: cant find sound driver for Portege r205-s209

 

Portege R205-S209

 

This one should work just fine. It's for machines in the same part number family.

 

   SoundMAX Integrated Digital Audio Driver for Windows XP/2000

-Jerry
Channel 9
Occasional Contributor
Posts: 17

Re: cant find sound driver for Portege r205-s209

Yup, Jerry, that driver seems to be the same one that is running on my R205-S209. OP: let me know if you have problems, and I'll take a closer look if it helps.

Posts: 45,932
Topics: 81
Kudos: 8,225
Solutions: 3,088
Registered: ‎12-04-2008

Re: cant find sound driver for Portege r205-s209

Thanks for the confirmation.

-Jerry
Channel 9