Windows 7 for Equium M70-337E?

Reply
Member
Posts: 1

Windows 7 for Equium M70-337E?

Just installed Windows 7 Premium (32 bit) on my trusty M70 and managed to get all the drivers I needed except the WiFi and Network Controller, I believe the wifi is a "Realtek RTL 8139/810 fast family Ethernet" or "Intel(R)PRO wireless 2200BG Network Controller".

   I've tried both the Vista 32 and 64 bit drivers without any joy. Any info where I might get a suitable driver would be appreciated.

Thanks John

Frequent Advisor
Posts: 8,209

Re: Windows 7 for Equium M70-337E?

[ Edited ]

Since Toshiba doesn't support that model under WIndows 7 you'll need to get the driver directly from the chipset manufacturer's support site. 

 

Also, try Unknown Device Identifier 7.00 to see if it can lead you to the proper driver.  http://www.zhangduo.com/udi.html

 

Since that is a European model you might have better luck posting on the European Support Forum where they actually sell that model instead of here in the USA forum where they don't. 

http://forums.computers.toshiba-europe.com/forums/index.jspa

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.