01-08-2012 04:34 PM
We are having trouble with my wife's Satellite A305 laptop (Windows Vist 64) and I want to run the PC Diagnostic tool that is supposed to have come with it. When I go to: Start -> All Programs -> Toshiba -> Utilities the program is not there. Is it on the recovery disks? If so what is the name of the program? If it's not on the disk can it be downloaded? All we could find on the Toshiba site was version for Windows XP. Where canI get this tool so I can run it?
Thanks,
Spence
01-09-2012 08:11 AM
Try C:/Program Files (X86)/Toshiba/PC Diag/PCDiag. If you have any further questions, please post your COMPLETE model number. It's on a label on the bottom of the machine. Looks like A305-XXXXX.
01-11-2012 06:04 PM
Hello,
Thanks for responding. I did not find the diagnostice tool. There is no "PC Diag" subdirectory in the "c:/Program Files (X86)/Toshiba/" directory. The full model number is Satellite A305-S6858.
Thanks,
spence
01-12-2012 07:26 AM - edited 01-12-2012 07:29 AM
You may also have a folder named Program Files without the (X86). If so, maybe it is there. There is no Download that I can find on the official Toshiba download site located here:
I have no idea where else to look. And I don't think it would be on the recovery disk since the specs for your machine doesn't show it as installed at the factory.
01-12-2012 05:49 PM
Thanks so much for you help. I was unsuccessful at locating the utility. I search the whole disk and it's not there. I guess I will look into a 3rd party diag tool.
thanks,
spence
01-13-2012
04:25 AM
- last edited on
01-13-2012
01:42 PM
by
Peter
Skeller,
You can find the Toshiba PC Diagnostics Tool by going to the download section and looking at the available downloads for your model and OS.
You'll see something called: Toshiba Value Added Pack
It might be abbreviated as: TVAP
Download and install it -- at the install you'll have a choice of what features to install, and the Toshiba PC Diagnostics Tool is one of those features.
Now you have it.
Regards,
The
HOSTINGDUDE
Cheap Domain Names
Cheapest Web Hosting
[Moderator edit to remove off-topic links.]
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.