03-14-2012 06:59 PM
Hi,
I'm not sure if this is posted in the right forum but....
I just purchased a Toshiba E305-S1995 laptop, and by "just" I mean today. I was personalizing my desktop and I chose one of those pre-selected desktop themes that used Aero features and everything was fine. I performed a couple of updates for Windows 7 as well as some through Toshiba Service Station.
Now I'm getting an error message that says: The current video card may support Aero with a driver that is compliant with the Windows Display Driver Model (WDDM). Contact the manufacturer of your computer or video card for a WDDM-compatible driver.
Does anyone know how to fix this? I tried doing the Windows updates like it suggested but I still have the same problem. Any suggestions on how to fix this, preferably step by step if at all possible?
These are the specs I pulled from the website if they help at all:
Processor3 and Graphics4
• Intel® Core™ i5-2410M Processor
o 2.3 GHz (2.9 GHz with Turbo Boost Technology), 3MB Cache
• Mobile Intel® HM65 Express Chipset
• Mobile Intel® HD Graphics with 64MB-1696MB dynamically allocated
shared graphics memory
Solved! Go to Solution.
03-15-2012 12:07 PM
03-15-2012 12:34 PM
That fixed the problem!! Thanks so much, Jerry ![]()
11-19-2012 06:22 PM - edited 11-19-2012 06:29 PM
Hi Jerry
Just looking for solution to why ReelTime "stops working". I have DX735-ST5N01 All n 1 desktopI have so many things, but cannot find the answer to why ReelTime installs successfully, but when I right click open (or) right click run as admin. The only thing that opens is the initial small pop up box with program name; then nothing happens. Troubleshooter says its a compatibiliy issue, but already tested it as well.
Any thoughts, advice, links, or direction on more trouble shooting, is greatly appreciated maybe it takes a certain Windows program for it to run?
DNice![]()
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.