05-09-2011 05:33 PM
I just installed Windows 7 Ultimate on my Toshiba R835-P56X. I have finally been able to install all the drivers that show up in the Device Manager. However, if I go to System Information > Components > Problem Devices it shows one device with PNP Device ID ACPI\TOS6208\2&DABA3FF&1. What is this and how do I take care of it?
Thanks.
10-18-2012 09:53 PM
HI. I have the Toshiba X505-Q888 with Windows 7 Ultimate 64bit. I have the same unknown driver with the same code. Did you ever find out which driver/software this is? I can't find it anywhere. Thanks.
10-19-2012 11:31 AM
You must have upgraded the hard way. When you use Windows Anytime Upgrade, drivers are undisturbed. And it takes only minutes.
Upgrade to another edition of Windows 7 by using Windows Anytime Upgrade
10-19-2012 06:38 PM
Turns out, in my case, the issue was the Bluetooth driver was not installed correctly.
I wound up using the program: Driver Utilities
It found the bluetooth driver was missing and it also found a few other things that were a bit outdated. I'm pretty happy, actually, with how it all turned out.
I found other posts, where it was the HDD Protection driver not installed correctly. IN my case, again, not this, but the B/T driver.
For what it's worth.
Thanks
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.