Uninstalling Toshiba Bulletin Board

Reply
Member
Posts: 4

Uninstalling Toshiba Bulletin Board

I'm trying to figure out how to uninstall the Bulletin Board app -- have tried a number of different uninstaller programs, and it doesn't seem to get recognized by those programs.  At the very least, I would like to stop it from autostarting, but again, it doesn't even show up as a program that gets autostarted.  Can someone shed some light on how to get rid of this program?  Thanks!

Posts: 4,809
Topics: 56
Kudos: 1,535
Solutions: 370
Registered: ‎05-03-2009

Re: Uninstalling Toshiba Bulletin Board

Control Panel/Programs and Features/Right click Toshiba Bulletin Board/Click Uninstall. You didn't bother to give us the model number and OS so I'm assuming you have Windows 7.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 4

Re: Uninstalling Toshiba Bulletin Board

Hi - thanks for the reply.  Yes, I am running Windows 7, and I did try the Programs and Features in Control Panel -- but the strange thing is that the Toshiba Bulletin Board is not listed among the programs.  All of the other Toshiba programs are there, but not Bulletin Board. 

Posts: 4,809
Topics: 56
Kudos: 1,535
Solutions: 370
Registered: ‎05-03-2009

Re: Uninstalling Toshiba Bulletin Board

I don't see how it could be active on your machine and not be listed in Programs and Features but I assume you are sure it's there. You didn't say why you are so adamant about not having it.  It's on both of my machines and has never caused any problem. Do you believe it is causing you some kind of harm?

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 4

Re: Uninstalling Toshiba Bulletin Board

It doesn't show up in Programs and Features (or in Revo Uninstaller or in IOBit's uninstaller).  But it definitely is running -- the notification icon shows up in the taskbar, and TosReelTimeMonitor.exe shows up as a running process in Task Manager. 

 

It doesn't cause any problems, but it does take up some memory, and I just prefer not to have extraneous programs running in the background. 

 

Member
Posts: 4

Re: Uninstalling Toshiba Bulletin Board

ah - I found a way to get rid of the program.  First, I installed the newest version from the Toshiba support site, rebooted, and then immediately uninstalled it. 

 

Anyway, thanks for the quick responses.  Hope this helps other readers. 

Posts: 4,809
Topics: 56
Kudos: 1,535
Solutions: 370
Registered: ‎05-03-2009

Re: Uninstalling Toshiba Bulletin Board

[ Edited ]

I'm glad you made it, Ted. However, I must tell you that the file you mentioned (TosReelTimeMonitor.exe) has absolutely nothing to do with Toshiba Bulletin Board.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit