Toshiba eco Utility--watt hours vs. kilowatt hous

Reply
Member
Posts: 2

Toshiba eco Utility--watt hours vs. kilowatt hous

The Toshiba eco Utility history shows watt hours (Wh) for the daily power consumption and shows in the upper left hand corner of each graph watt hours.  The watt hours for the monthly and weekly make sense for the months or weeks shown.  The amount for the daily graph does not seem to add up to the current day or days shown and is a mystery number.  When one mouses over any day on the daily graph, one gets watt hours as seems appropriate.  However, when one mouses over the months or weeks one still gets a number that says watt hours but is actually kilowatt hours.  These two graphs need to be fixed to note "Kh" not "Wh".