Toshiba U400 10N - Windows XP wifi driver problem ! [SOLVED]

Reply
Member
Posts: 6
Accepted Solution

Toshiba U400 10N - Windows XP wifi driver problem ! [SOLVED]

[ Edited ]

Hi I have installed windows xp proff Toshiba u400 10N PSU40E with SATA support using nLite.

installed drivers downloaded from toshiba and intel driver pages.

Everything works fine except my wifi connection.

Intel Wireless WiFi Link 4965AGN

Everest sees it but it is not in device manager and other intel driver setups not working just.

When i clicking on exe it just won't open.

Also Intel(R) ICH8 Family PCI Express Root Port 6 - 2849 is marked in device manager.

 

Intel® Wireless LAN Identification Utility

says that

 

"Wireless LAN Hardware and Driver Version:Wireless LAN Hardware not detected.
Possible Causes:
No Wireless LAN hardware is installed.
The Wireless LAN hardware installed cannot be detected by this utility."

 

 

tried these driver setups.

XPDriver12.4.0.21.1.x32_wCAT

wlan-intel-3495-4965-v1240211-xp

 ICS_Dx32.exe

 ICS_x32.exe

 

 

Need help !

 

 

[PROBLEM SOLVED] 

After Bios update wireless problem was solved.


Accepted Solutions
Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

After BIOS update problem was solved. Smiley Happy

View solution in original post


All Replies
Frequent Advisor
Posts: 8,208

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Check your owners manual to see if you need to turn the WIFI on.  I know my L305-S5933 has a switch in the front to turn it off and on and some models used the Function Keys to turn the Wifi on and off. 

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.


Posts: 47,493
Topics: 83
Kudos: 9,025
Solutions: 3,198
Registered: ‎12-04-2008

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

i have already downloaded these files.

 

When i click on Setup.exe inside XPDriver12.4.0.21.1.x32_wCAT

it just does not starts. Onyl see clock on mouse then after seconds it dissappears.

I think there is a conflict with wireless.

 

 when i click on iProDifX.exe inside XPDrv folder under XPDriver12.4.0.21.1.x32_wCAT

opens a dialog panel Now performing driver installation then it dissappears too.

 

Posts: 47,493
Topics: 83
Kudos: 9,025
Solutions: 3,198
Registered: ‎12-04-2008

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Use the zip file from my source instead. Decompress wlan-intel-3495-4965-v1240211-xp.zip into an empty folder.

 

If Setup.exe does not work properly, then try running it from Safe Mode (where the VGA driver is in use).

 

   A description of the Safe Mode Boot options in Windows XP

 

If that doesn't work either, install from Device Manager as follows.

 

Boot into Safe Mode, go to Device Manager (devmgmt.msc), expand Display adapters, right-click on the display device, and click Update Driver.

 

Guide the Hardware Update Wizard to the w29n51.inf file in the ..\XPDriver12.4.0.21.1.x32_wCAT\XPDrv folder.

-Jerry
Channel 9
Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

tryed safe mode advices

does no worked.

 

formatted c and reinstall windows

 

here the snapshot when installing chipset driver

it comes until port 6 then problem

wifilink shows on traymenu

after restart it dissappears/

weird situation/

Smiley Indifferent

i see

Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Reforma and reinstall windows several times today.

with various combinations.

tryied to install drivers before SP3

and after SP3 still got problem with Wifi link .

 

After SP3 installed i got Blue Screen when installing chipset driver

on subinstalling Intel(R) ICH8 Family PCI Express Root Port 6 - 2849 

 

here is blue screen error report details 

 

 

and here is how Everest sees the Wifi Link on port 6

 

 

Posts: 47,493
Topics: 83
Kudos: 9,025
Solutions: 3,198
Registered: ‎12-04-2008

Re: Toshiba U400 10N - Windows XP wifi driver problem !


Reforma and reinstall windows several times today. with various combinations.

tryied to install drivers before SP3 and after SP3 still got problem with Wifi link . 


Try it this way. Install Windows and before anything else install the following Intel software in this order.

   Storage Manager

   Chip Set Utility

   Display Driver 

 

Then try the Wireless LAN Driver before SP3.

 

All the Toshiba drivers and utilities are here.

-Jerry
Channel 9
Frequent Advisor
Posts: 8,208

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Try it without Service Pack 3.  There are a lot of WiFi issues with XP SP3.  Try it with SP2 and see if that helps.

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.


Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

i tried with SP2 

i tired to formatting ...have so many works...

tomorrow i will try with jerry last installation order

Member
Posts: 6

Re: Toshiba U400 10N - Windows XP wifi driver problem !

After BIOS update problem was solved. Smiley Happy

Frequent Advisor
Posts: 8,208

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Great news.  Thanks for letting us know.

-------------------------------------------------------------------------------------

If you don't post your COMPLETE model number it's very difficult to assist you. Please try to post in complete sentences with punctuation, capitals, and correct spelling. Toshiba does NOT provide any direct support in these forums. All support is User to User in their spare time.


Posts: 47,493
Topics: 83
Kudos: 9,025
Solutions: 3,198
Registered: ‎12-04-2008

Re: Toshiba U400 10N - Windows XP wifi driver problem !

Glad to learn that. Thanks for reporting it.

-Jerry
Channel 9