Reply
Member
SebastianB
Posts: 1
0
Accepted Solution

Toshiba Satellite L755-S5306

Alright, I just signed up here because I need help with something, I'm not sure if I'm posting this in the right place, so please forgive me. Also, I'm kind of a dunce once it comes to computers, so you guys will probably know tons more than, so hopefully I don't annoy anyone.

Anywho, onto business. I scanned my computer using Avast! the free version, and I noticed that it had scanned a little bit over 500G's of data, which I realized to myself was impossible, since my hard drive says it has a maximum capacity of 449G. I thought that was strange so I looked up how much space my computer SHOULD have on Toshiba's website, and it said that my computer should have a 500G harddrive. So now I'm confused, I can't find any sort of secondary hard drive at all, and the only other thing in my "Hard Disk Drives" Section is this Microsfot Office Click-to-run 2010 (protected) Q: I checked that out and it said it has 0 bytes, so I'm pretty sure that the missing 51G isn't hiding in there.

Besides that fact, even if I do have the missing 51G's somewhere, there's still the fact that my Avast! managed to scan over 500G of data.

So, I guess my question is, did I do something wrong with my computer? It is broken in any way?

Super Advisor
cbwilsha
Posts: 2,573

Re: Toshiba Satellite L755-S5306

[ Edited ]

Well, Sebastian, lots of folks have that question so don't be embarrassed for asking. You will have to ask Avast how they manage to scan more than is there.

 

Windows says a Gb is 1,073,741,824 bytes while the manufacturer says a Gb is 1,000,000,000 bytes. The manufacturer is going by the metric system and Windows is going by a computer design standard.

So on a 500,000,000,000 byte drive the
Manufacturer calls it: 500,000,000,000 divided by 1,000,000,000 =500Gb
Windows calls it: 500,000,000,000 divided by 1,073,741824 = 465.66Gb

 

You can see then that you really had about 466 GB to start with.  And with Toshiba computers, there is a about 1.5GB partition which controls the HDD recovery process and about a 15 GB partition that is the full back up of your out-of-box computer. 466 GB-15 GB-1.5 GB = 449.5 GB for your C Drive. You can see the exact partitions on your machine by typing Disk Management in your Start/Search box and then clicking on Create and Format HD Partitions. That will open Disk Management showing all partitions on your HDD.

 

You have nothing to worry about and even the Avast count may be an anomaly that doesn't occur again. Now, enjoy your computer!

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit
Ace Advisor
Jerry_Lippey
Posts: 33,083
0

Re: Toshiba Satellite L755-S5306


Windows says a Gb is 1,073,741,824 byte

Just to clarify a bit more, that difference is because the drive manufacturers talk in decimal while programmers talk in binary.

 

The number above is 2^30 instead of 10^9.

 

See my attachment.

-Jerry