Toshiba Satellite A505-S6005 PCI Bus Enumerator

Reply
Member
Posts: 2

Toshiba Satellite A505-S6005 PCI Bus Enumerator

I bought a Toshiba Satellite A505-S6005 and clean installed Windows 7 Ultimate to get rid of the third party software and other junk. I have a problem with one of the devices in the evice manager. It reads as PCI Simple Communications Controller and I have narrowed it down to the PCI Bus Enumerator by looks at the Physical ID. I can't seem to find the correct driver to install this device on the toshiba website. Any suggestions?

Posts: 47,052
Topics: 83
Kudos: 8,929
Solutions: 3,170
Registered: ‎12-04-2008

Re: Toshiba Satellite A505-S6005 PCI Bus Enumerator

 

Satellite A505-S6005 

 

Probably the chipset software.

 

The order of installation often matters. Always run the chipset installation utility followed by the display driver prior to other drivers.

-Jerry
Channel 9
Member
Posts: 2

Re: Toshiba Satellite A505-S6005 PCI Bus Enumerator

Can you point me to the correct Chipset driver for the A505-S6005 because i originally installed it first and thought PCI Simple Communications Controller meant the modem.

Posts: 47,052
Topics: 83
Kudos: 8,929
Solutions: 3,170
Registered: ‎12-04-2008

Re: Toshiba Satellite A505-S6005 PCI Bus Enumerator

[ Edited ]

Yes, I expect it's not the chipset. More likely a modem or Ethernet adapter.

 

Is anything not working?

 

   Troubleshoot Unknown Devices In Device Manager Of Windows 7

 

These look like the right ones.

 

   Intel Chipset SW Installation Utility for Windows XP/7 (32/64)

 

   Intel Display Driver for Windows 7 (64)

-Jerry
Channel 9
Member
Posts: 1

Re: Toshiba Satellite A505-S6005 PCI Bus Enumerator

[ Edited ]

Toshiba Supervisor Password v. 2.00.03PLV AKA util_su_password_25675A.exe I attached the file. I hope that's not against the rules...

 

Runit and away goes your unknow device!