09-14-2012 11:06 AM
Hi, I Have a Qosmio X775 3DV78 running windows 7. I am looking for the software/driver that that gives the ability to use the buttons by the power key like using the volume keys, enabling wifi etc. I am also looking for the software to enable the use of the function key. Anyone know the name of the files I have to download ?
09-14-2012 12:08 PM
Have they ever worked?
C.B.
09-14-2012 12:28 PM
Yes they worked, I just had to reinstall windows 7 and need the name of driver to download from the toshiba website. I believe it is "Toshiba Value Added Package" That has the drivers ?
09-14-2012 12:44 PM
Assuming your Windows 7 is 64 bit, HERE is the TVAP driver and HERE is a future reference for ALL the drivers for your machine.
C>B.
09-14-2012 12:59 PM
I just had to reinstall windows 7..
Best to restore the hard disk to its original out-of-the-box contents using Toshiba recovery media. No need to struggle with drivers and utilities.
See the section Restoring from recovery DVDs/media, which begins on p. 76 of the User's Guide.
Qosmio X770 Series User’s Guide
If you did not create the recovery media, you can obtain it from Toshiba.
If you want to upgrade Windows 7, this is not the way to do it.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.