Toshiba Driver TSST corpCDDVDW TS-L633C TF20

Reply
Member
Posts: 4

Toshiba Driver TSST corpCDDVDW TS-L633C TF20

 

I've a problem with my DVD

 

Just burned DVD/CD, reading white/new cds/dvds

but when I try de read these cd/dvds, it isn't working, it doesn't find cds/dvds.

 

I don't know if the problem is the region, because I live in Peru.

 

Before, I try unistall drivers, reboot,and working, but now, isn't.

 

DRIVER: TSST corpCDDVDDW TS-L633C TF20

MODEL NAME: TSST corpCDDVDW TS-L633C

VERSION: TF20

OEM code: TF

 

LAPTOP

MODEL: Satellite C655-S5140

 

OS: Windows 7 - 64 bits.

 

Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba Driver TSST corpCDDVDW TS-L633C TF20

Victor, try the suggestions in this article.

 

What can I do if my CD or DVD drive doesn't work properly in Windows 7?

- Peter
Member
Posts: 4

Re: Toshiba Driver TSST corpCDDVDW TS-L633C TF20

Thanks Peter,

 

I try that!!!

 

PD: Do you believe if the problem is the firmware? 

Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba Driver TSST corpCDDVDW TS-L633C TF20

I'm not sure what the cause is unfortunately.

- Peter