Some FN keys not working on L875D-S7332

Reply
Member
Posts: 2

Some FN keys not working on L875D-S7332

[ Edited ]

I am unable to use some of the FN keys on Satellite L875D-S7332, purchased in Nov. It is running Windows 8.

 

My husband did some uninstalling & reinstalling and the keys stopped working.

 

The following FN + F? key combinations do work - F4 (display), F9, F10, F11 (volume & mute)

 

The following DO NOT work - F2, F3 (display brightness), F5 (touchpad), F12 (wifi adapter). I also do not see the flashcard lineup of all FN keys & their function when I press one that works.

 

We did install TC30511200D from Toshiba drivers.

 

Is there a TVAP or something similar for a S7332 that would restore the complete FN keys functionality.

 

Thank you.

 

-amy.

Posts: 47,981
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: Some FN keys not working on L875D-S7332

 

Satellite L875D-S7332

 

Downloads here.

 

 

Amy what happens if you install the earlier version of the utility, before it was rewritten to include 32-bit Windows?

 

   Toshiba Function Key (Version 1.00.25 - Released Date 08/14/12)

-Jerry
Channel 9
Member
Posts: 2

Re: Some FN keys not working on L875D-S7332

Jerry,

 

thank you for the reply. When I try to install the older version (1.00.25) over the newer (TC30511200D), I get the message that a newer version of the software is already installed.

 

So I uninstalled the newer & installed the older.

 

The screen brightness controls worked once, I had to close the laptop lid for a few minutes, when I reopened it, the brightness controls ( F2 & F3 ) and wifi (F12) do not work, but the other F keys seem to be working.

 

I tried reinstalling 1.00.25 again, no difference, any other suggestions ?

 

I rebooted my laptop and found that the  FN+F2 & FN+F3 keys work for a few seconds after the reboot and then they stop working.

 

Also, I am familiar with the S7332 downloads page link you sent earlier, but there are too many downloads listed and I don't know which ones really beneficial. If there is a critical toshiba driver that I should have installed, please let me know. At present the only toshiba programs listed under "Programs and Features" is the "TOSHIBA Function Key".  I welcome any suggestions.

 

thank you.

 

-amy.

 

Posts: 47,981
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: Some FN keys not working on L875D-S7332

Sometimes resetting the computer has proved fruitful.

 

With the battery and AC adapter removed, close the Power switch for 30 seconds.

-Jerry
Channel 9