09-28-2010 03:23 AM
model no: PSLBGG-01Y00N
I want the drivers for windows 7. Webcam is not working for me. Previously I used xp it didn't had any problems but in windows 7 its not working.
I also want the other drivers also.
Like, the sound is much low in windows 7 without the driver than what I used to get in windows xp.
09-28-2010 08:05 PM
It's an Indian machine. I can find drivers from Toshiba only for 32-bit Vista and Windows XP. Are you interested?
09-28-2010 09:48 PM
Yes I'm interested but the thing is that whether drivers for Windows 7 for this model is available or not. If u have the drivers for Xp or Vista plz give the link.
Thanks.
09-29-2010 12:17 PM
For the 32-bit Windows Vista and XP drivers and utilities, go here and look up the Satellite L300.
Toshiba India Download Drivers
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.