Satellite A665-S6086 Drivers

Reply
Member
Posts: 3

Satellite A665-S6086 Drivers

Just replaced the hard drive, I have Windows 7 64 bit, can't seem to find the drivers for it.  Went to the Drivers section but it seemed to be mostly for Windows 8.

Posts: 47,632
Topics: 84
Kudos: 9,081
Solutions: 3,209
Registered: ‎12-04-2008

Re: Satellite A665-S6086 Drivers

 

Satellite A665-S6086

 

Downloads here.

 

 

Best to restore the hard disk to its original out-of-the-box contents using Toshiba recovery media. All the drivers and utilities are properly preinstalled. Windows is preactivated.

 

If you failed to burn recovery discs, you can obtain them from Toshiba. Scroll down to Get Recovery Media here.

 

For instructions, see the section Restoring from recovery DVDs/media, which begins on p. 73 of the User's Guide.

 

   Satellite A660 Series User’s Guide

-Jerry
Channel 9
Occasional Advisor
Posts: 16

Re: Satellite A665-S6086 Drivers

http://support.toshiba.com/support/modelHome?freeText=2759671

 

There are more than 124 drivers for Windows 64bit Windows 7 on that page and only 80 for Windows 8. 

Please explain your congressional definition of most and in exchange i'll tell you that I can't tell a difference in speed and performance whether I use Microsofts or Toshiba's installed version of Windows.

 

Now, if I'm using the same magical logic you used to count, would you heed my advice?

"hello, hello, IS THIS THING ON ?!?!!??!!! --Mr. Tinkles "