Reply
Occasional Contributor
Posts: 14

SOLUTION:Toshiba updates too slow to download, and with only one file at a time.

[ Edited ]

 

SOLUTION:

 

Toshiba updates via Toshiba Service Station are unacceptably slow to download, and with only one file at a time.

 

To bypass the slow downloads, to be able to download multiple updates simultaneousy, and to keep permanent copies on your hard drive do the following steps:

 

- Open Toshiba Service Station.

- Note the name and release number for each update.

- Open the web page http://support.toshiba.com/support/drivers and make sure the list of updates covers many months.

- Do a text search for the update name, and especially the version number.

- Click on that update

- Click on download

- OPEN/click that downloaded file to install updates

- Repeat for each update.

 

...

Occasional Contributor
Posts: 14

Re: SOLUTION:Toshiba updates too slow to download, and with only one file at a time.

[ Edited ]

You can also do update/driver searches via google and entering the name and version number from Tosh Service Station.

Member
Posts: 1

Re: SOLUTION:Toshiba updates too slow to download, and with only one file at a time.

This is ridiculous. Toshiba can we have a response please!. we all dont have the time to wasting time downloading the updates one by one rather than through the service station portal. Why is is so SLOW!