Reply
Occasional Contributor
Yahweh
Posts: 13
0

Modem Device on High Definition Audio Bus Driver

[ Edited ]

Realtek Audio Driver for Windows XP(v5.10.0.5599; 10-31-2008; 49.1M)

 

 

 

I got Satelite L305-S5919 and i just wan't to know if this is the right driver for it 'Cause I already installed this but in device manager under other devices this modem device on high definition audio bus there is yellow "?" tnx in advance :smileywink: by the way i got XP OS

 

 

EDIT:

NVM,just find the right driver i thought it's really needed:smileysurprised:

Ace Advisor
Jerry_Lippey
Posts: 33,074
0

Re: Modem Device on High Definition Audio Bus Driver

 

Satellite L305-S5919 

 

This one looks right to me.

 

   Realtek Audio Driver for Windows XP

 

This one on the European site should work too.

 

   Realtek Sound Driver for Windows XP, 5.10.0.5599, 08/09/08

-Jerry
Member
MrToshi
Posts: 1
0

Re: Modem Device on High Definition Audio Bus Driver

I hope to prevent others from having to endure the same annoyance looking for this driver that I have had.

 

My problem with Modem Device on High Definition Audio Bus Driver could not be solved with audio drivers. This is because the device is a modem, as the alert says.

 

I could not find the drivers for the modem on ANY Toshiba or Realtek website <- this is unfortunate. Luckily the website www.findthatfile.com still stores the modem drivers.

 

Visit www.findthatfile.com and search for mdm-20080410072404.zip

 

The file mdm-20080410072404.zip contains the drivers for this modem.

Member
de-lic
Posts: 2
0

Re: Modem Device on High Definition Audio Bus Driver

hi , does this acually work im scare to download :/

Member
de-lic
Posts: 2
0

Re: Modem Device on High Definition Audio Bus Driver

hi does this really work ?