Lost network drivers after installing Windows7

Reply
Member
Posts: 2

Lost network drivers after installing Windows7

I have Toshiba laptop (Satellite U505-S2925BN), upgraded from vista to Win7, every thing is working fine except when I checked the drivers on the device manager I found a question mark under other devices and when I open it I found 4 drivers missing: Base system Device (2 times), Network Controller, and unknown device. I also noticed that my wireless is not working it is not detecting my router and I can not connect to internet any more. When I click on the question mark I got this message "The drivers for this device are not installed (Code 28)" I have tried to find these drivers on Toshiba site with no help. All drivers are available except this one..any idea what could be the problem??

Regular Advisor
Posts: 231

Re: Lost network drivers after installing Windows7

Go to this site and click the link "Download Toshiba Software Installer for Windows 7 now". Install the software and hopefully it will find the missing drivers for your system.

Member
Posts: 3

Re: Lost network drivers after installing Windows7

Don't know if you noticed but the prob was no internet access. You have to have internet access for those solutions to work.

Posts: 47,962
Topics: 85
Kudos: 9,136
Solutions: 3,232
Registered: ‎12-04-2008

Re: Lost network drivers after installing Windows7

 

Satellite U505-S2925BN

 

I would use the Ethernet connection instead. If it doesn't work either, download this driver using another computer (the one you're using now) and transfer it.

 

   Realtek LAN Driver for Windows 7 (32/64)

-Jerry
Channel 9