How to determine running BIOS version, Satellite A665-S6058?

Reply
Member
Posts: 1

How to determine running BIOS version, Satellite A665-S6058?

Toshiba Service Station is telling me that a new BIOS is available, however, the button tells me : Reinstall instead of Install.

 

How do I determine the BIOS version currently running in my Satellite (which, by the way, works fine -- no problems. I don't wish to create any by reinstalling a BIOS that may not be needed.)?

Posts: 4,923
Topics: 57
Kudos: 1,721
Solutions: 388
Registered: ‎05-03-2009

Re: How to determine running BIOS version, Satellite A665-S6058?

[ Edited ]

Start, type "System" in Search Box, click on System Information in listing above.

 

BTW, if you aren't having any problems that a BIOS update is designed to fix, I advise you to leave well enough alone.  If it ain't broke, don't fix it.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit