Drivers Windows XP SP2 - Satelllite L635-S3050

Reply
Member
Posts: 3

Drivers Windows XP SP2 - Satelllite L635-S3050

Greetings to all,

 

Recently acquired one of its products which criterizei the quality of it, it's a Notebook L635-S3050, which came with Windows 7 installed.
With my old notebook I used Windows XP SP2 for some programs that I use does not run on Windows 7.
The fact is that after formatting and installing Windows XP SP2 on this laptop, I noticed that the toshiba website (http://www.csd.toshiba.com) found no drivers available for download.
I wonder if you can make them available on the website, or using Internet links to download.
Thank you in advance,
Klayton de Oliveira
Recife - PE - Brazil

 

 

Super Advisor
Posts: 1,472

Re: Drivers Windows XP SP2 - Satelllite L635-S3050

[ Edited ]

They already have drivers for XP service pack 2 available for that model.

 

http://www.csd.toshiba.com/cgi-bin/tais/support/jsp/modelContent.jsp?ct=SB&os=&category=&moid=275979...

Click the downloads tab and then use the drop down menu to select XP service pack 2

 

 

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement
Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Drivers Windows XP SP2 - Satelllite L635-S3050

 

Satellite L635-S3050 (PSK00U-02R02X)

 

This US site has only half-a-dozen or so XP drivers and utilities, but the European site has several dozen for the following models, which are in the same part-number family. They should work just fine.

 

   Satellite L630-xxx (PSK00E-xxxxxx)

 

Those drivers are here.

 

Install the Intel chipset software followed by the Intel display driver prior to any other drivers. Install the Common Module before any other Toshiba utilities.

-Jerry
Channel 9
Member
Posts: 3

Re: Drivers Windows XP SP2 - Satelllite L635-S3050

Hello friends,

Thanks for the posts, but it seems that the computer did not sit well with Windows XP.

He worked for a week and stopped showing error with blue screen, I thought it was the drivers who had installed before, so with your help, formatted again and installed the drivers listed.

Result tou he'll submit the bug with three weeks of use.

Well, the customer decided to use the same Windows 7.

How do I get the recovery discs from toshiba?

Where do I call?

Thank you in advance,

Klayton de Oliveira
Recife - PE - Brazil

Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Drivers Windows XP SP2 - Satelllite L635-S3050


How do I get the recovery discs from toshiba?

They will ship to South America.

 

   Order Toshiba Recovery Media

-Jerry
Channel 9
Member
Posts: 3

Re: Drivers Windows XP SP2 - Satelllite L635-S3050

Hello Jerry,

You have the option to download?

Can I download from here.

Thank you in advance,

Klayton de Oliveira
Recife - PE - Brazil

Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Drivers Windows XP SP2 - Satelllite L635-S3050

So far as I know, Klayton, you can only order the optical discs and have them shipped.

 

   Order Toshiba Recovery Media

-Jerry
Channel 9