Driver for installation of Windows 7

Reply
Member
Posts: 3

Driver for installation of Windows 7

[ Edited ]

I wanted to install fresh Windows 7 installation on new HDD, from Toshiba. Everything went good, till Windows installator couldn't find drivers for CD/DVD...?, without it I can't continue, selecting the DVD with Windows installation or clicking Rescan, doesn't work. Where can I find these drivers to include on DVD, so I can proceed with installing Windows.

(asked on answers.microsoft.com and forums.toshiba.com)

 

Bootmenu says the HDD is: TOSHIBA MQ01ABF032.

 

[It's code 19, when installing for CD/DVD, where can I download these drivers?]

[Only HDD is from Toshiba]

Posts: 47,680
Topics: 85
Kudos: 9,089
Solutions: 3,214
Registered: ‎12-04-2008

Re: Driver for installation of Windows 7


Only HDD is from Toshiba


So you don't have a Toshiba computer?


Windows installator couldn't find drivers for CD/DVD


Maybe this message?


A required CD/DVD drive device driver is missing. If you have a driver floppy disk, CD, DVD, or USB flash drive, please insert it now.


If so, see this Microsoft article.

   "A required CD/DVD drive device driver is missing" or "A media driver your computer needs is missing...

-Jerry
Channel 9
Member
Posts: 3

Re: Driver for installation of Windows 7

It didn't help.

 

  • Burn the installation DVD at a slower speed.

It pops error.

  • Use a better quality DVD to create the installation DVD.

This is good quality DVD.

  • Update the BIOS firmware for your DVD drive.

My BIOS is blocked, same as admin (other problem, I'll be left myself with).

It requires UAC (User Access Point?), which admin, so...

Posts: 47,680
Topics: 85
Kudos: 9,089
Solutions: 3,214
Registered: ‎12-04-2008

Re: Driver for installation of Windows 7

This forum is for Toshiba computers, Rik. Best of luck in your (Dutch) Microsoft thread.

 

   Installator requires drivers that aren't there

-Jerry
Channel 9