09-19-2012 11:37 AM
I'm running Windows Vista 6.0, Build 6002. The CD/DVD device will not operate. The Device Manager shows the message "This device cannot start. (Code 10)".
I've tried to obtain a driver update but only find utilities to scan and repair that cost money. I should be able to solve this without an purchased utility program.
Any advice is appreciated.
Thanks you.
Solved! Go to Solution.
09-19-2012 12:18 PM
Always tell us which computer you have. See the label on the bottom.
Description of Code 10-related errors that Device Manager generates in Windows-based computers
09-20-2012
11:36 AM
- last edited on
09-24-2012
12:12 PM
by
Peter
My computer is:
Satellite A305-S6852
Model PSAG0U-03K00L
Serial XXXXXXXXX
Thanks.
[Moderator edit to remove serial number.]
09-20-2012 12:01 PM
09-20-2012 05:26 PM
I just tried Microsoft Fixit. It didn't resolve the problem. It said the driver had to be reinstalled. I have the original disc for the Toshiba but expect I can't use it since the CD/DVD drive does not start.
What suggestions do you have?
Thanks.
09-20-2012 05:31 PM
One way to find out if the device is malfunctioning is to use the driver in the BIOS.
Locate a known-good bootable disc and try booting from it.
Load the disc, restart the computer, press F12 at the Toshiba screen, set the boot priority, and see what happens.
09-22-2012 05:07 PM
I tried to boot from the manufacturers disc and was able to do so. So the drive functions. But it seems all I can do from that disc is to recover the whole system which would wipe out my data.
How do I get a new driver? When I click on Update Driver for the CD/DVD in the Properties window for the device, the system responds that I have the latest driver.
Thanks
09-22-2012 06:56 PM
Try this Fix it.
Your CD drive or DVD drive is missing or is not recognized by Windows or other programs
09-24-2012 08:28 PM
I can't burn an audio disc or play an audio disc.
09-25-2012 10:37 AM
I followed the instructions in the last Fix It you suggested, did the manual registry changes (deleted two entries), restrated the computer and the problem was resolved!
Thanks!!
09-25-2012 01:13 PM
Interesting. That registry situation doesn't usually produce Code 10.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.