Bluetooth RFBUS Problem

Reply
Member
Posts: 4
Accepted Solution

Bluetooth RFBUS Problem

Hi all, i seem to be having an issue with my RFBUS driver, when i trouble shoot, it comes back with an error code 10. i have absolutely no idea where to go from here Smiley Mad. if anyone could point me in the right direction i would greatly appreciate it! thanks!

 

computer specs:

Toshiba Qosmio x775-Q7380

Intel Core i5-2430M CPU @ 2.40 GHz

6GB Ram

64 bit operating system

 

Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem

Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

You might try earlier versions. If it's the driver install that failed, for instance, try this one.

 

   Intel Bluetooth Filter Driver

 

There are also earlier versions of the Stack compatible with Windows 7.

 

And you can try installing in Safe Mode.

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem

 

Qosmio X775-Q7380

 


when i trouble shoot, it comes back with an error code 10.


Please attach a picture of that.

 

In the meantime, try reinstalling the Bluetooth stack.

 

   Bluetooth Stack for Windows by Toshiba

-Jerry
Channel 9
Member
Posts: 4

Re: Bluetooth RFBUS Problem

ok, so i uninstalled the bluetooth stack and attempted to reinstall the latest version, however about halfway through i encountered a message stating that my device driver software did not sucessfully install... i included a picture to better describe the situation. after the installation finished, i returned to the devices and printers window and again troubleshooted my pc only to find the same error code ten (picture also included). Any ideas?

Thanks for your time!


Member
Posts: 4

Re: Bluetooth RFBUS Problem

*Update*  

If it helps.. i went to the device manager window and found bluetooth RFBUS and under its properties, the device status box it says "This device cannot start. (Code 10)" (included picture).

 


Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem

 

   Code 10: The device cannot start

 

Let's install the Bluetooth driver and then the stack (again).

 

   Atheros Bluetooth Filter Driver Package

 

   Bluetooth Stack for Windows by Toshiba

-Jerry
Channel 9
Member
Posts: 4

Re: Bluetooth RFBUS Problem

success! thanks alot! it seems to be working now many thanks!

Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem

You're welcome. Happy to help.

-Jerry
Channel 9
Member
Posts: 1

Re: Bluetooth RFBUS Problem

hello ... I have the same problem with my pc ... I have not tried to do everything and not work ... maybe I can help...                                        

 

 

Toshiba NB515-SPO201RL


Member
Posts: 1

Re: Bluetooth RFBUS Problem

hi, im interest this topic

i have same trouble in my toshiba satellite pro c640 windows8 x64 operating system.

im already download adn update many driver, well no one work.

 

help me please


Occasional Contributor
Posts: 11

Re: Bluetooth RFBUS Problem

I have the very same problem as you suhar80y. Did you get any help?
Member
Posts: 3

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

Protege Z30-A1302.  Win 7 Pro, 64Bit.  I have unistalled Atheros and the Stack repeatedly, following those with a registry cleaing with Ccleaner.  I have had no success.  I get the same messages: error 10, Bluetooth not ready, etc. My screen shots would be the same as others have posted. the installer files are for the laptop I have.

Ken

 

LibrarianK

see Kafka

Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

 

Portege Z30-A1302

 

Downloads here.


..Atheros...


Your Bluetooth is Intel. Install in this order.

 

   Intel Bluetooth Filter Driver

 

   Bluetooth Stack for Windows by Toshiba

-Jerry
Channel 9
Member
Posts: 3

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

Hi Jerry. Thanks for near-instant reply.  RFBUS element failed. I used your links to get to correct files (strike key, replace user).Be away 4abit.
tc00621600a.exe installed with no dialog boxes and was done in under 2 seconds. That seems too easy, even though it is a relatively small install. The fail came late in the stack install.  I ran both 'run as Administrator' I deleted, cleaned up and tried again tc00621600a install took longer (more of a normal experience) and had dialog boxes display.  However RFBus failed again. 
I may not have suspended-shutdown all security software, but absent an explicit warning, shouldn't running the installs as Administrator be enough?  Following security software used: Norton Internet Security suite, and Malware Bytes.
 
Jerry, what can you suggest as a next step?  Any antecedent drivers/software to un- re-install? Stubbornly persevere blindly?
I have just a few Bluetooth devices and all worked fine at some previous time.
  
Thank you,  
LibrarianK
 
Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

You might try earlier versions. If it's the driver install that failed, for instance, try this one.

 

   Intel Bluetooth Filter Driver

 

There are also earlier versions of the Stack compatible with Windows 7.

 

And you can try installing in Safe Mode.

-Jerry
Channel 9
Member
Posts: 3

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

Bingo. The Older version you syggested solved the issue. Thank you Jerry  Well done.

LibrarianK

Posts: 46,777
Topics: 83
Kudos: 8,795
Solutions: 3,145
Registered: ‎12-04-2008

Re: Bluetooth RFBUS Problem: Reinstalls Don't fix

You've been without Bluetooth for all that time? Happy to hear it's fixed.

-Jerry
Channel 9