Question
The Camielio S20/H30 does not charge as outlined in the Owner's Manual. Is the camera defective?
Answer
When charging your Camileo S20 or S30 camera using a USB cable or the AC adapter, the charge indicators may not respond as stated in the USER’s GUIDE. This information is to inform you of possible variations in the operation of the indicators during charging.
Indicators
Camileo S20
AC Adapter
When charging your Camileo S20 using the supplied AC adapter, both indicators may flash while charging. You may be able to operate the camera while connected, but charging may stop while in use. When the battery is fully charged, both indicators may illuminate steady for 5 minutes, then turn off.
USB
When charging your Camileo S20 using a USB Cable connected to a computer (computer on or using a Sleep and Charge enabled port with the computer in sleep mode), both indicators may flash one time, then the Blue camera indicator remains illuminated steady while charging. You may not be able to operate the camera while connected and/or charging the camera using a USB cable. When the battery is fully charged, the indicators may remain illuminated until the USB cable is disconnected.
Camileo S30
AC Adapter
When charging your Camileo S30 using the supplied AC adapter, both indicators may flash once, then both remain illuminated steady while charging. You may be able to operate the camera while connected, but charging may stop while in use. When the battery is fully charged, the indicators may illuminate steady again for up to 5 minutes, then turn off.
USB
When charging your Camileo S30 using a USB Cable connected to a computer (computer on or using a Sleep and Charge enabled port with the computer in sleep mode), both indicators may flash one time, then both remain illuminated steady while charging. You may be able to operate the camera while connected and/or charging the camera using a USB cable, but charging may stop while in use. When the battery is fully charged, both indicators may remain illuminated until the USB cable is disconnected.
Charge Time
AC Adapter
Depending on the battery charge state when started and battery condition, charge time for Camileo S20 and S30 cameras when connected to the supplied AC adapter may be up to 5 hours.
USB
Depending on the battery charge state when started, battery condition and USB supply voltage / current of the connected port, charge time for Camileo S20 and S30 cameras when connected to a computer using a USB cable may be up to 11 hours.