Reply
Member
wesleywong
Posts: 5
0

Toshiba Value Added Package

i have satellite L655....

what is the use of 

  • Toshiba Value Added Package? do i need to install for my laptop?

 

Occasional Contributor
Schnauzer
Posts: 44
0

Re: Toshiba Value Added Package

[ Edited ]

You should already have this installed.

 

Control Panel --> Programs and Features, and see if you can find Toshiba Value Added Package in the Programs List.

 

This package contains several diagnostic utilites, as well as Power Management Capabilities, which I believe are not exactly perfect.

 

However, it also contains the utilites which let's you use the FN function keys that control Display Brightness, etc etc...

 

 

Member
wesleywong
Posts: 5
0

Re: Toshiba Value Added Package

i ady check my program list...

where got tis package...

my fn key function well no problem at all...

if i install it, any pro and con?

Member
fofang13
Posts: 2
0

Re: Toshiba Value Added Package

Pro's:

Extra features

More options

 

Con's:

Takes up space

You probably don't need it depending what you want it for

Member
deamonkiller56
Posts: 1
0

Re: Toshiba Value Added Package

do you need it if you only use your computer for the internet 

Frequent Advisor
drev9
Posts: 1,061
0

Re: Toshiba Value Added Package

I usually keep my installs to a mimimum on my computers, but the TVAP is one that I always install.  The use of the function keys, and all of the functions that they provide are worth it IMHO.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9600, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i5-450M, HM55, 8GB RAM, Intel 710 SSD (travel system)
Member
robie1der
Posts: 9
0

Re: Toshiba Value Added Package

if tvap is so good why is it not preinstalled

Frequent Advisor
drev9
Posts: 1,061

Re: Toshiba Value Added Package

It is preinstalled on Toshiba laptops

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9600, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i5-450M, HM55, 8GB RAM, Intel 710 SSD (travel system)