05-10-2011 02:16 PM
Be gentle, since I'm not very technical.....
I was preparing my rarely used Netbook (XP version) to give to my elderly father & installed AVG with current virus definitions with no problem. When I went to upgrade to the current version of Firefox, it hung. When I tried to reboot, it wouldn't & started clicking. From what I've been told, the hard drive probably crashed & needs to be replaced. Any other ideas?
If that's all it is, will any SATA 2.5 work & can I go to 7200 vs 5400? Since I never created a restore disc (no CD drive), do I have to buy from Toshiba?
And are there directions for replacing the hard drive, since I hope to do it myself?
Thanks!
Karen in Texas
05-10-2011 04:33 PM
Which NB205, Karen?
I've attached some pictures to help you replace the disk. You will re-use the existing caddy ("plate" in the picture).
You will need to order the recovery discs from Toshiba.
03-17-2012 12:14 PM
What size torx wrench/drive do I need to remove the cover on the NB205 to access the HDD and where can I purchase the correct tool?
04-30-2013 04:40 AM
I saw this old thread, and thought I'd post here.
It seems the HDD on my Toshiba NB205 has died. I never backed it up, but no big loss of data. However, I have no recovery disks that I know of, nor do I have an external dvd drive.
So, even if I buy and install a new HDD, how would I get Windows installed, and all the Toshiba software installed?
Thanks
04-30-2013 07:28 AM
Next time you post on the Forums, please start your own thread rather than piggy back on another--in this case, one over a year old! Recovery Media is also available in USB form. I'm not sure about your specific machine. Go HERE and scroll down to order.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.