04-10-2012 07:33 AM
> In the beginning I am going to say that I own a Satellite L650 notebook
> with a Mobility Radeon HD 5650 graphics, which I couldn't find on the
> "select your model" list. I would like to ask if there is any way to
> obtain/download diplay driver for my card, because the only one, published
> here [ http://ce.computers.toshiba-europe.com ] or here [
> http://support.amd.com ] are not up-to-date since 14th January 2011 or
> so. Trying to download the driver from Toshiba Europe even the "auto
> detect" tool failed to recognize my notebook and graphic card and it says
> that my display driver is not up-to-date. I am writing with my problem
> directly here, because I could not find any help in the Internet.
> Everything would be ok, because my notebook works perfectly, but only
> problem is the display drivers and almost all games work at horribly low
> Frame Per Second rate [ 20-30 FPS ] during the gameplay, and some of them
> won't even run. Sometimes a HUD disappears, charecters blink/lag, some
> stuff goes overbright, or colors are "negative". I would be mostly grateful
> if You could update drivers publisheb on the [
> http://ce.computers.toshiba-europe.com ] website or send me separate link
> for them or just me the driver to my e-mail address. I enclose my
> notebook's full specification from [ http://www.csd.toshiba.com ] website
> and full diagnostics (32 bit and 64 bit) from the DxDiag tool
04-10-2012 07:19 PM - edited 04-10-2012 07:20 PM
Can't help you. You have the most recent update available from Toshiba. Toshiba is notorious for not regularly updating their drivers. They only update them when there is some proven instability issue. This is the bane of Toshiba owners who are gamers like you, who need regular video driver updates. I can only suggest you send a polite but strongly worded letter to Toshiba.
Mike
04-11-2012 04:25 AM
Thank you for your answer, Mike! ![]()
I would send'em a letter, but I live in Poland, so it would cost me more money than it's worth. No more Toshiba, no matter what, and no more notebook, only PC : D
Tommy.
04-11-2012 04:50 AM
You're very welcome, happy to help. Sorry I couldn't give you better news.
Mike
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.